Error Code

Index.Sub 603F.0H
Data Type Unsigned16
Access Read Only
PDO Mappable TX_PDO (1)
Unit --

Range

--
Default Value 0
Store Supported No
Description

This object captures the code of the last error that occurred in the drive.

Value (hex)

Description

0000 hex

No error

FF01-FFFF hex

Manufacturer specific

Notes

  •              (1) available with firmware V00r74 or superior.